SCHUNK at Metalloobrabotka

Unique component selection for equipping your robots and machine.

Metalloobrabotka is a major trade show of the global machine tool industry and state-of-the-art metalworking technology. Over 30 years the exhibition has brought together leading manufacturers, suppliers and dealers from around the world. Today, Metalloobrabotka hits the world top ten trade shows in the machine tool industry. SCHUNK, the competence leader for gripping systems and clamping technology, demonstrated how visitors can fully exploit their machine and system performance and benefit from the perfectly coordinated interplay of gripping systems and clamping technology. Visitors had the chance to hand shake with our servo-electric 5-finger hand. Amongst others, SCHUNK highlighted its new flagship for quick-change pallet technology, VERO-S NSE3. The set-up time optimizer is 100% compatible with NSE plus 138 and has an optimized design for even higher system rigidity. 

SCHUNK welcomed Aleksandr Mostovoi

About 4 weeks before Soccer World Cup, SCHUNK welcomed Aleksandr Mostovoi on the booth.

The famous russian soccer player was, amongst others, U21 European Champion with the Soviet Union, Soviet Champion 1991 with Spartak Moscow and UEFA Champion Intertoto Cup 2000 with Celta de Vigo. 

SVH 5-Finger Hand

The SVH 5-finger hand received the German Social Accident Insurance (DGUV) Certificate for safe, collaborative operation.


SCHUNK, the competence leader for gripping systems and clamping technology has succeeded in taking a decisive step towards safe human/robot collaboration: as the world's first robot gripper, the SCHUNK SVH 5-finger hand has been certified and approved by the German Social Accident Insurance (DGUV) for collaborative operation.
At our booth, visitors had the once in a lifetime chance to shake the future by the hand.

Product details

Our product highlights

VERO-S NSE3 138

The high-performance pneumatic quick-change pallet system for universal milling operations.

Positioning and clamping in one single operation – VERO-S gets to the heart of rationalization. The set-up time killer ensures higher machine running times, and a more rational production from batch size 1. The new premium modules are fully compatible with the previous VERO-S modular system, which now consists of more than 1,000 possible combinations for highly efficient workpiece clamping.

  • 100% compatible with NSE plus 138 for easy replacement of the modules.
  • Optimized design for even higher system rigidity.
  • Increased pull-in force thanks to optimized module kinematics in every clamping position.
  • Optional cone seal for fully protected clamping bolt interface.

Go to special

Hydraulic compensation jaw

Chuck jaw with oil chamber system for low-deformation workpiece clamping.
  • Centrifugal force compensation for safer clamping due to lower loss of clamping force.
  • Low-deformation clamping of thin-walled or sensitive workpieces.
  • Vibration dampening for improved workpiece surface quality.
  • Adjustable concentricity for maximum accuracy in machining.

Product details

TENDO Slim 4ax

The world's first slim hydraulic expansion toolholder in standardized heat shrinking contour as per DIN 69882-8.

Slim heat shrinking contour outside – clever hydraulic expansion technology inside! With the SCHUNK TENDO Slim 4ax, it has been possible for the first time to unify the complete external geometry of heat shrinking mountings with the convincing qualities of SCHUNK hydraulic expansion technology.

  • Standardized heat shrinking contour in accordance with DIN 69882-8
  • Tool change within seconds without peripheral equipment
  • 100% work safety or zero risk principle for tool clamping
  • Plug & Work guarantee: 1:1 interchangeable. Insert a hydraulic expansion toolholder – replace a heat shrinking toolholder. Ready for immediate use!

Go to special

ROTA NCA power lathe chuck

Sealed power lathe chuck for significantly longer maintenance intervals.
  • Permanent grease lubrication
    for consistently high clamping forces.
  • Large toolholder through bore
    for processing all conventional bar diameters.
  • Weight-optimized design
    for significantly reduced acceleration and braking times.

Product details

Component and equipment finder clamping technology

More than 7,500 components for your tool and workpiece clamping. Select your machine.

Soccer World Championship 2018

Our highlights in Russia
SCHUNK tipster game
Autograph cards signed by
Jens Lehmann
Autograph cards signed by
Aleksandr Mostovoi
Contact person

Internal sales

 

You have a question on the technology, price or delivery time? Our internal staff is looking forward to hearing from you.
Your in-house contact persons

Service and support

 

Your direct contact Tel.: +7-812-326-78-35
Service overview