FAQ

You enter bets for the results of all matches from the opening match to the final. The goal is to win as many points as possible and become the overall winner - and this is what you have to do:

Place your bet

You can enter a bet up to the time when the game kicks off. The kick-off times are shown on the 'Bet' page. After that, the betting closes and no further bets are accepted even if the start of the match is delayed. Your bet is only valid if you have selected a result for each of the two teams.
You must predict the match result including all goals from extra time and penalty shoot-out.

My team

Select your favourite team and collect points together with your teammates

Every player can join their favourite team. The points in the fan league are calculated the same way as the ranking calculation of the betting communities.

It is always possible to change your favourite team.

Challenge

A challenge is a betting duel on a matchday.

You can challenge any player by visiting his/her profile and clicking "Challenge". A window will open, in which you can select different matchdays. A challenge must be re-initiated for each matchday. Every player can have up to 8 challenges.

All betting duels are listed for each matchday on the Challenge page. There you can see against whom you have won or lost. The duels do not influence the betting game rankings, but are listed in a separate ranking.

Examples Points allocation challenge

On his challenge account, the winner of a challenge is credited with the opponent's points that he has won. In case of a draw, the points are split and each of them receives the points that they have achieved.

Points obtained in the betting game Points for the challenge rankings
Player 1 Player 2 Player 1 Player 2
9 6 6 0 Player 1 receives the points from the opponent
9 10 0 9 Player 2 receives the points from the opponent
9 9 4,5 4,5 Points split

The challenge points are added for each player. This produces a challenge rankings list.
The current score is displayed for each participant in a ranking list that is sorted by score.

Extra bets

The extra bets can be entered up to 14.06.2018 at 20:00. The number of points for the correct answer can be found next to the question on the extra bets page.

The points are on the final day separately added to the total score.

Each selected answer can be correct and can result in points.

Invite

The Invite page gives you the opportunity to invite friends. Enter the email address to which an invitation is to be sent. The free text can be chosen freely.

You can also invite your guests directly to a betting community that you have joined. To do this, enter the selected betting community into the form. The person invited then automatically becomes a member of the betting community.

A second option is to publish on Facebook. Subsequently, the invitation appears on your Facebook pinboard.

Cancelled matches

Cancelled matches or matches without a result will be completed later and are then entered in the rankings. The winnings distribution will, however, not be affected by this. Under certain circumstances, the winner will be thus be determined among fewer players.

Other points

The organiser cannot be held responsible for any technical problems or transmission errors that may occur. The player accepts this condition when he registers to play. Manipulations of any type will result in immediate disqualification.