arrow calendar cartcheck checkmark close configure contact danger download external_link facebook globeinfo instagram jobfinder linkedin logo_claim logout mail menuminus navigation pin play plus rss searchshaft success twitteruserwarning wechat x-twitterxing youku youtube zoom
Change the country selection to see information on the products, services and contact persons that are relevant for your location.
Tool clamping technology

Vise automation lowers the barrier to entry

SCHUNK's new vise automation system makes it easy to get started with automated machine loading and unloading. Precise positioning and clamping, simple robot programming, and a manageable capital expenditure ensure reliable processes and longer machine running times.

Vise automation The VERO-S 1-way clamping station as a console version enables high-precision positioning and clamping of the vises in a single operation.

The requirements for machine automation vary depending on the workpiece, batch size, manufacturing process, and desired flexibility. SCHUNK therefore does not pursue a universal solution approach but offers a tiered portfolio of different types of automation: from simple entry-level to high-end solutions. Based on extensive application experience and a broad portfolio of clamping and automation components, SCHUNK enables tailored, process-oriented automation concepts. The new vise automation system expands this range with a particularly simple entry-level option: it offers companies a straightforward and low-risk way to automate loading processes quickly, cost-effectively, and with minimal integration effort.

Positioning and clamping in a single operation

Vise automation is based on a deliberately simple concept: workpieces are manually clamped into specially prepared vises outside the machine and then loaded into a storage rack. A robot equipped with special gripping fingers picks up the loaded vises and positions them precisely on a raised VERO-S 1-way clamping station on the machine table of the machine tool. After machining, it returns them, along with the workpiece, to the storage rack. Re-clamping for machining the underside of the workpiece can take place both outside and inside the storage rack.

At the heart of the vise automation system is the VERO-S clamping station as a console version. It serves as the interface between the robot and the machine tool, and enables high-precision positioning and clamping of the vises in a single operation. Thanks to the high pull-down forces and the micrometer-precise interface of the quick-change pallet system, the robot consistently picks up and changes the clamping devices with repeat accuracy. The raised console version provides optimal accessibility for machining five sides of the workpiece. At the same time, the quick-change pallet module is completely covered by the clamping device. This prevents chip buildup and ensures consistently high process reliability. Depending on the machine type, the console version can be operated either via the machine or via the robot.

Vise automation Using special gripper fingers, the robot removes the loaded vises from the storage rack and places them back there after machining.

The critical clamping process remains under the operator's control. The robot is responsible solely for the reliable handling of the complete vise. Since it always uses the same defined interface and moves to fixed positions, programming is reduced to simple point-to-point movements. This significantly reduces the complexity of automation and makes it easier to integrate into existing manufacturing systems. Since no media feed is required on the machine side, the automation system can be used flexibly with virtually any type of machine.

Longer machine running time, lower investment

Vise automation can significantly extend machine running times. Before the end of their shift, machine operators can prepare several loaded vises in the storage rack. The machine will then continue to operate autonomously even after work hours. This allows companies to increase their productivity without having to employ additional staff.

At the same time, they benefit from a comparatively low capital expenditure. The entire system consists of standardized components and, thanks to its clearly defined interfaces, is easy to program and operates reliably. The combination of low complexity, high process reliability, and cost-effective implementation makes vise automation an attractive entry point into automated machine tending.

Watch the video for more details

Download press releases

Press releases 2 MB ZIP Download