arrow calendar cartcheck checkmark close configure contact danger download external_link facebook globeinfo instagram jobfinder linkedin logo_claim logout mail menuminus navigation pin play plus rss searchshaft success twitteruserwarning wechat x-twitterxing youku youtube zoom
Changez la sélection du pays pour voir les informations sur les produits, les services et les interlocuteurs pertinents pour votre localisation.
Success Stories dicembre 2025

Automation of end-of-line processes for stable series production

High and standards, short cycle times, maximum process reliability – the requirements of the automotive industry leave no room for compromises. To meet these requirements, the EMS provider SVI Austria, together with SCHUNK Electronic Solutions and other partners, opted for a fully automated overall solution. The result: a future-proof manufacturing solution that combines efficiency and quality.

SCHUNK 2-finger gripper A SCHUNK 2-finger gripper grips the printed circuit boards from the intermediate station and deposits them into the test nests.

At its Austrian location, SVI, a globally operating EMS provider, employs 350 people who work on a production area of 5,300 square meters to actively shape the future of automotive electronics production. With the goal of further expanding its expertise and specialization in this field, SVI Austria aims to set new standards as a strong partner for its customers.

SCHUNK SVI Austria Peter Lazarus, Operator at SVI Austria (left), Stefan Lorenz, Area Sales Manager (DE/AT) at SCHUNK Electronic Solutions (middle), Walfred Krienzer, Manager Manufacturing & Test Equipment at SVI Austria

The challenge: precision, efficiency and reliability

Before working with SCHUNK Electronic Solutions, SVI Austria relied on stand-alone solutions and manual work at the end of the line. However, the demands on the processes increased – both in terms of volumes, and regarding to quality and process reliability. The existing structure reached its limits. A fully automated seamless solution became necessary. “We wanted a solution that could handle our growing production volumes while ensuring the quality of our products,” Walfred Krienzer, Project Manager at SVI Austria. “Above all, it was important to us to minimize manual intervention and remain flexible.“

The solution: an innovative overall line concept

4-position magazine loader ILR-2800 The 4-position magazine loader can hold up to 23 panels per stack and transfers them to the ILR-2800 depaneling machine.

SCHUNK Electronic Solutions, together with strong partners such as Achat5 Engineering GmbH – an expert for board handling solutions, Schnaidt GmbH – a specialist for equipment for electronics manufacturing, and Dr. Eschke Elektronik GmbH – a recognized expert in test systems, developed a highly automated production line that covers all process steps.

The process started with a 4-position magazine loader capable of handling up to 23 stacks of panels. These panels are then gradually transferred into the ILR-2800 via an intelligent board handling system – synchronized with a processing cycle. In this context, SCHUNK and Achat5 have further intensified their partnership: in the future, SCHUNK will offer Achat5’s board handling systems as part of its own portfolio – providing even more integration from a single source.

The ILR-2800 is the heart of the line, impressing with maximum precision at top speed. Two specially developed SCHUNK linear axes, extending across the entire machine, enable particularly efficient cycle times. On these axes are four positions for the workpiece carrier shuttles, which operate perfectly in sync with a time offset. This ensures continuous processing with virtually no waiting times and maximizes productivity. The workpiece carrier, developed and manufactured in cooperation with Schnaidt, as well as the complete lid station, are equipped with SCHUNK’s VERO-S quick-change pallet system – providing secure fixation and fast, precise changeovers. This is a decisive advantage for process reliability.

lid station VERO-S quick-change pallet system The lid station is equipped with a VERO-S quick-change pallet system and provides highest separation quality.

The process flow in detail:

  • Position 1 loading: A SCHUNK gripper precisely places the panel on the product-specific workpiece carrier.
  • Position 2 lid station: The circuit board is equipped with a lid that remains securely fixed by the VERO-S quick-change pallet system. This ensures stability throughout the entire separation process.
  • Position 3 milling process: The milling process runs in a highly automated and efficient manner: A 6-position tool changer enables one week of operation without manual intervention. Functions such as hold-down device, tool breakage and diameter control, and milling brush monitoring ensure consistently precise results. Different milling depths reduce wear, while the dust-reduce booster ensures an almost dust-free separation. After milling, the workpiece carrier is automatically returned to the lid station.
  • Position 4: The separated printed circuit boards are picked up by a SCHUNK gripper and placed onto an intermediate station with two slots. This intermediate station then transfers the boards to the rotary indexing cell for the ICT test. After all boards have been placed, the shuttle with the workpiece carrier returns to position 1, where a vacuum gripper picks up the remaining edge and disposes of it in a garbage bin located in the lower machine area. The process then starts again from the beginning.

Maximum utilization – minimum downtime

The sophisticated design of the ILR-2800 enables virtually uninterrupted processing. The combination of synchronized workflows and seamlessly integrated process steps – from milling to lid placement to disposal – ensures maximum machine utilization with the highest process stability.

Rotary indexing cell: quality assurance at its highest level

rotary indexing cell ICT test In the rotary indexing cell, the ICT test is carried out, while additional processes could be implemented at the idle positions.

The rotary indexing cell was developed together with Schnaidt GmbH and Dr. Eschke Elektronik GmbH. It performs the in-circuit test (ICT) and ensures consistently secured product quality. “The ICT test is a central part of our production process,“ Walfred Krienzer. With the specially developed C-adapter and precisely manufactured test nests, the printed circuit boards are securely fixed during the test and checked for electrical functionality. “The seamless integration of the test saves time and reduces sources of error,” Krienzer continues.

Efficiency in palletizing: The PAL-1500

After the testing process, the SCHUNK palletizing system PAL-1500 takes over the inspected printed circuit boards. Functions such as tray centering, ejection station, and empty tray control ensure a smooth and secure transfer to the next production stage. A separate reject parts conveyor provides safe handling of faulty components without interrupting the production flow.

Thanks to its modular design, the PAL-1500 can be flexibly adapted to different tray formats and offers maximum process reliability – particularly important for series production in automotive industry.

Seamless communication: MES and SMEMA connection

The production line is fully MES-capable, enabling central control and end-to-end traceability. SMEMA interfaces facilitate seamless data exchange between the machines, while scanner and set-up controls further enhance process reliability. “To meet the requirements of the automotive industry, this seamless communication is indispensable,“ emphasizes Krienzer.

Conclusion: future-proof production thanks to automation

The production line implemented at SVI Austria exemplifies successful partnership and intelligent automation. With a planned annual output of up to 4 million products, the system sets new standards in efficiency and quality. “The system operates exactly as planned, and the effort required for operation and set-up was significantly lowered than expected – this makes the entire process even more efficient,” summarizes Krienzer. Stefan Lorenz, Sales Representative at SCHUNK Electronic Solutions, adds: “The system’s flexibility allows additional processes such as laser marking or hot staking to be seamlessly integrated – perfectly tailored to the requirements of our customers.”

The automotive industry is facing challenges, but also great opportunities. Highly automated production processes are increasingly essential for securing long-term quality, scalability, and competitiveness.