arrow calendar cartcheck checkmark close configure contact danger download external_link facebook globeinfo instagram jobfinder linkedin logo_claim logout mail menuminus navigation pin play plus rss searchshaft success twitteruserwarning wechat x-twitterxing youku youtube zoom
Změňte výběr země, abyste získali informace o produktech, službách a kontaktních osobách, které jsou důležité pro vaši lokalitu.
Company

Efficiency meets precision: clamping and automation solutions for every production process

The future of metalworking is flexible, precise and automated. At EMO Hannover 2025, SCHUNK will be demonstrating how flexible clamping devices, modular automation concepts and global engineering expertise support companies in making their processes efficient and future-proof.

SCHUNK CPS EMO Depending on the workpiece, batch size, production process and machine, SCHUNK offers users a choice of different types of automated machine loading - from simple entry-level to high-end solutions.

How can companies future-proof their processes in times of global uncertainty, increasing competitive and cost pressure and a shortage of skilled workers? More than ever, this question is occupying the minds of those in the metalworking industry. EMO Hannover, the world's leading trade fair for production technology, is to provide some answers. At the SCHUNK booth, visitors can expect practice-oriented production modules with which parts handling and processing in the machine can be made even simpler, more flexible and more resource-efficient.

Efficient automation of the machine tool

Automated loading and unloading is a decisive lever for increasing productivity and efficiency in the manufacturing process. But which automation solution suits which production process? The application specialist provides orientation and offers a wide range of automation solutions that are precisely tailored to the requirements with regards batch sizes, workpieces and production processes. The focus is not only on providing users with the right components, but also on supporting them with sound expertise and the right step sfrom the outset ].

New clamping solutions for versatile application

In addition to automation, SCHUNK also offers all modules for versatile and low-setup workpiece clamping in the machine. For the machining of complex workpieces or small batch sizes, the company is presenting new clamping solutions that are specially tailored to the requirements of flexible production environments.

KSC-5X SCHUNK The new KONTEC KSC-5X 5-axis centric clamping vise with a unique range of system and top jaws ensures optimum accessibility during machining, even with complex workpieces.

With the KONTEC KSC-5X , SCHUNK is expanding its family of 5-axis vises with a high-performance centric clamping vise. It has been especially developed for demanding machining operations. Its higher base jaws, combined with a selection of system and top jaws that is unique on the market, enable complex workpieces to be clamped with optimum accessibility. Thanks to a spindle quick-change system, the vise can be quickly and easily adjusted to new clamping tasks. Thanks to the integrated interface of the quick-change pallet system, it fits seamlessly into the extensive modular clamping technology system, which enables a wide range of possible combinations for highly efficient workpiece clamping.

SCHUNK ROTA THW3 2+2 Absolute flexibility in workpiece clamping: The new power-operated ROTA THW3 2+2 compensation chuck with jaw quick-change system reliably clamps different workpiece geometries - from round and square to complex shapes.

SCHUNK is also clearly moving in the direction of flexibility with its lathe chucks. Following on from the manual chucks, a 2+2 jaw compensation chuck is now also available for power chucks. Thanks to its innovative drive concept, the new ROTA THW3 2+2 power chuck enables the centrically compensating workpiece clamping of any geometry - from round and cubic to bulky parts. Equipped with a patented seal and permanent lubrication as well as a jaw quick-change system, it manages the balancing act between low maintenance and short set-up times while offering consistently high clamping forces.

Customized with SCHUNK Engineering

Every production process is unique, and standard solutions are not always the best choice. SCHUNK supports users with a structured process for the development of customized solutions. SCHUNK accompanies its customers from the precise definition of requirements through design, to production and integration - and thus creates bespoke solutions that are precisely tailored to their production requirements in various industries. For example, precisely fitting hydraulic clamping devices for turbine rotors in the aerospace industry are validated and optimized using digital simulation tools.

Standardized turnkey solution

GROW Marking SCHUNK SCHUNK standardizes entire processes such as laser marking and parts separation within a modular system. GROW Marking enables users to laser important information such as serial numbers precisely and permanently onto products.

While customized developments are indispensable for complex requirements, small and medium-sized companies in particular require practical concepts that can be implemented quickly. This is where SCHUNK comes in with the new modular GROW automation cells . These turnkey, CE-certified complete solutions are intuitive, flexibly adaptable and have been specially designed to automate manufacturing processes quickly and efficiently. Whether for laser marking or part separation - GROW enables companies to optimize their production without extensive prior knowledge and to benefit from high reliability and scalability.

Data-based process control in real time

NSE3-PH 138-V1-K IOL Product image Variant Electrically actuated quick-change pallet modules with fully integrated electronics and actuators: Thanks to a wide range of monitoring and transmission options, the VERO-S NSE3-PH 138 IOL offers greater transparency in the clamping process - without additional interfering contours.

With the increase in automation and the digitalization of machine tools, the focus is increasingly shifting to the intelligent monitoring of processes. Electrical and sensor-based clamping systems from SCHUNK make it possible to monitor the process-relevant status of the clamping devices and workpieces or the vibration behavior of the tools in real time. As a result, they not only offer greater safety and end-to-end transparency, but also simple integration into existing machine control systems - an important basis for the production of the future. An absolute highlight will be the battery-operated clamping devices, which can be integrated wirelessly, e.g. by radio, via solutions from common measuring system providers or via IO-Link wireless. Visitors will have the chance to see the benefits of these technologies for themselves in a live demonstration at the SCHUNK booth.

Visit SCHUNK at the EMO: Hall 3, Booth I26

Stáhnout tiskové zprávy

Tiskové zprávy 6 MB ZIP Ke stažení